Two production sites in Europe
The headquarters of Lapp Mobility GmbH are in Stuttgart. This is where the central administration and the production of Mode 2 charging cables and Mode 3 cables for retail and infrastructure in the Low Volume - High Mix concept are located. Thanks to the proximity to development, sales, product management and the laboratory, the team in Stuttgart can quickly develop and implement customer-specific solutions.
All major car manufacturers are supplied from the Otrokovice site in the Czech Republic. The current portfolio consists of AC charging solutions with a focus on the Mode 3 charging cable. The location corresponds to the high-volume, low-mix approach with large quantities per variant.
Thanks to the two differently oriented locations, Lapp Mobility can offer both a high degree of customization and the production of large quantities. The central location in Europe also guarantees European customers short transportation routes and therefore fast delivery times and a positive CO2 balance.
Lapp Mobility Stuttgart
Central administration and production site
Oskar-Lapp-Str. 2
D-70565 Stuttgart
GermanyLapp Mobility Otrokovice
Production site
Bartošova 315
765 02 Otrokovice - Kvítkovice
Czech Republic