Questions and Answers
Traditional vehicles are colloquially known as "combustion engines." They use fuels like gasoline or diesel and burn them to power a combustion engine that provides energy for the vehicle. This process of burning fuel emits pollutants such as CO₂ and particulate matter, which are harmful to the environment and contribute to climate change. Alternative drives have been developed as more environmentally friendly alternatives to traditional combustion engines. Below are the most important alternative drives listed and briefly described:
- Electric Drive (BEV): Vehicles with electric motors and rechargeable batteries.
- Hybrid Drive: Combination of combustion and electric motors:
- Mild Hybrid: Assisted by an electric motor but cannot run on electricity alone.
- Full Hybrid: Can drive short distances purely on electricity.
- Plug-in Hybrid (PHEV): Larger battery, rechargeable externally, longer pure electric ranges.
- Fuel Cell Drive (FCEV): Hydrogen is converted into electrical energy, emissions are only water vapor.
- Natural Gas (CNG): Vehicles that run on compressed natural gas, less CO₂ emissions.
- Autogas (LPG): Vehicles with liquefied petroleum gas, also lower emissions.
- Biofuels: Made from biological materials like vegetable oil or ethanol, for modified combustion engines.
- Synfuels/E-Fuels (synthetic fuels): Made from renewable energy and CO₂, CO₂-neutral when using renewable energy.
- Solar Vehicles: Use solar cells for electrical energy, mostly for small vehicles or special applications.
- Hydrogen Combustion Engine: Modified engines that burn hydrogen, fewer emissions than conventional fuels.
BEV
- Advantages: Emission-free operation, high efficiency, quiet.
- Disadvantages: Battery production impacts the environment, charging infrastructure not as widespread as gas stations.
PHEV
- Advantages: Flexible, emission-free driving on short distances.
- Disadvantages: Heavier, lower efficiency due to higher weight.
FCEV
- Advantages: Fast refueling, long range.
- Disadvantages: High energy demand for hydrogen production, few refueling stations.
E-Fuels & Biofuels
- Advantages: Existing infrastructure and vehicles can be used.
- Disadvantages: Low efficiency, high costs, limited availability.
The availability of cars with alternative drive systems has increased, with electric cars (BEVs) and hybrids (full and mild hybrids) dominating the market, while natural gas vehicles (CNG) are no longer available as new cars due to lack of demand and the focus on electric mobility. The rising demand for electric cars is linked to a significant increase in new registrations, even though the purchase prices for pure electric vehicles are higher than for combustion engines. The charging infrastructure is being continuously expanded, even though government subsidies for electric cars have expired.
Current Trends in Alternative Drive Systems
- Electric cars (BEV): New registrations of electric cars are growing strongly, which is attributable to high demand and manufacturer investments in electric mobility.
- Hybrids (HEV, PHEV): Hybrid vehicles, especially full and mild hybrids, are also widespread and contribute to the increasing share of alternative drive systems.
- Natural gas/CNG: The trend is moving away from natural gas vehicles as manufacturers are turning away from this technology due to lack of demand and the focus on electric mobility.
- SynFuels/E-Fuels: Synthetic fuels (e-fuels) are not currently expected to become widely used in road transport due to their high costs and energy consumption, but are more likely to be used in heavy-duty transport in aviation and shipping.
Outlook
- The market for alternative drive systems will continue to shift in favor of electric and hybrid vehicles as manufacturers focus their attention on them.
- Price parity between electric cars and combustion engines is expected to be achieved for many models by 2030.
The ability to recharge or refuel cars with alternative drives (BEVs, PHEVs, FCEVs, CNGs, synthetic fuels, biogas) depends on the availability of infrastructure, which varies globally. BEVs and PHEVs are widely supported in urban areas and developed countries, while hydrogen (FCEVs), CNG, synthetic fuels, and biogas stations are limited to specific regions with active government support or renewable energy programs. Remote and less developed areas may lack sufficient facilities, so checking local infrastructure is essential before use.
Yes, there are significant differences in range between the various drive types, based on the characteristics of the energy sources, the efficiency of the drives, and the energy density of the fuels used. Here is an overview of the ranges of the various drive types:
BEV (Battery Electric Vehicle):
Between 200 and over 700 km range, depending on the battery size (e.g., 40 kWh to 100 kWh) and the efficiency of the vehicle. The range is also influenced by driving style, outside temperature, and the use of air conditioning/heating.PHEV (Plug-in Hybrid Electric Vehicle):
Usually between 30 and 100 km electric range, depending on the battery size. In combination with the combustion engine, the range is over 800 km.FCEV (Fuel Cell Electric Vehicle):
Usually between 400 and 800 km range, depending on the size of the hydrogen tank and the efficiency of the fuel cell.Combustion engines with e-fuels:
Similar to classic combustion engines, often between 600 and 1,000 km range, depending on the tank size and the vehicle.Classic combustion engines (diesel/gasoline):
- Diesel: Range between 800 and 1,000 km.
- Gasoline: Range between 600 and 800 km.
Conclusion:
- BEVs offer high efficiency and are ideal for short to medium distances, but are limited by the charging infrastructure.
- PHEVs combine flexibility with electric range, but are dependent on charging habits.
- FCEVs enable emission-free mobility with good ranges, but are limited by the hydrogen infrastructure.
- Combustion engines with e-fuels and classic combustion engines offer long ranges and fast refueling, but are less efficient and cause higher emissions (depending on the fuel).
An electric car registered in 2023 performs better after 45,000 kilometers compared to a gasoline car. Compared to a diesel car, it performs better even after 25,000 kilometers. The largest share of emitted CO₂ in E-cars is due to battery production. With new battery systems and increasing production, CO₂ emissions from new electric cars are continuously decreasing. Advantages of electric cars: No local emissions, low CO₂ emissions, higher energy efficiency.
Refueling a car with a combustion engine usually takes only a few minutes (typically 3-5 minutes) and enables a typical range between 600-1000 km depending on the size of the vehicle and driving style. When driving, the combustion engine produces CO₂ emissions and other pollutants that contribute to air pollution and climate change. Charging an electric car can vary depending on the type of charging station and the battery's state of charge.
- At a regular household socket (2.3 kW), it can be charged for several hours or overnight, with only a small range being recharged.
- At a fast-charging station (50 kW or more), charging to 80% capacity can take about 20 minutes to an hour. Typical ranges between 200-500 km are recharged, with the range depending on driving conditions (temperature, model, and driving conditions).
Charging the car is very similar to charging electronic devices. You drive to the charging station, park the car, connect the charging cable to the car and the charging station, and start the charging process. Payment is often made via apps, charge cards, or directly at the charging station, making it currently more complicated than at conventional gas stations. Unlike combustion engines, electric cars produce no direct emissions and are therefore more environmentally friendly in operation. However, the environmental balance also depends on the type of generated electricity (renewable energy vs. fossil fuels).
Manufacturers of electric cars specify the battery's capacity either in net or gross:
- Gross Capacity: This is the total capacity of the battery. It indicates how much energy the battery can store when fully charged.
- Net Capacity: This is the usable capacity of the battery. It is the amount of energy that can actually be used to operate the car. Part of the gross capacity is reserved to extend the battery's lifespan and prevent damage.
Simply put: The gross capacity is the total amount of energy the battery can theoretically store, while the net capacity is the amount you can actually use.
There are several methods available to suit varying needs and situations. Here are the main ways to charge an electric car:
- Home Charging
This is the most convenient and commonly used method for charging electric vehicles:
- at a standard household socket (up to 2.3 kW): Slow charging using a Mode 2 charging cable or the Mobility Dock. This is most suitable for charging overnight.
- at a private wallbox or a high-voltage socket (3.7–22 kW): Faster charging at home with a Mode 3 charging cable at a Wallbox or using the high-voltage connection with a Mode 2 charging cable.
- Public Charging Stations
Public charging networks are available in many urban areas, shopping centers, and highways for EV owners who need to charge while away from home. These include:
- Public AC Charging Stations (11–22 kW): Often found in cities at parking lots, shops, and corporate buildings. Charging is done via a Mode 3 charging cable that the EV owner carries along in the trunk.
- DC Charging Stations (50–150 kW): On highways and expressways. Charging with a permanently installed DC charging cable with CCS2 plug.
- DC High-Power Charging Stations (HPC) (150–350 kW): Extremely fast charging for long distances, mostly found on highways. Charging with a permanently installed DC charging cable with CCS2 plug.
- Workplace Charging
Many employers offer AC or even DC charging stations at the workplace for their employees. This option provides convenience and allows EV owners to charge their vehicles during working hours.
- Battery Swapping
Although less common, battery swapping involves replacing the depleted battery with a fully charged one at specialized stations. This is very fast compared to traditional charging methods. However, it requires compatible infrastructure and vehicles.
- Regenerative Braking
While not a direct charging method, regenerative braking helps recharge the battery slightly while driving. It converts kinetic energy into electric energy when the car is braking or decelerating.
Each charging method has its own benefits depending on factors like cost, convenience, and charging speed. Most EV owners use a combination of home charging and public charging stations to meet their daily needs.
AC Charging (Alternating Current):
- What is AC? AC stands for 'Alternating Current,' which is the type of electricity that comes from most home outlets.
- How does it work? During AC charging, the car is connected to a regular socket or a special charging station. The car has a built-in charger, also called an On-Board Charger (OBC), that converts the alternating current into direct current (DC) because the battery can only store DC.
- Speed: AC charging is usually slower. It's suitable for overnight charging at home or at public charging stations when you can park for longer periods.
DC Charging (Direct Current):
- What is DC? DC stands for 'Direct Current.' It is the type of current that directly flows into the car's battery.
- How does it work? During DC charging, the car is connected to a special fast-charging station. This station converts alternating current into direct current before it is fed into the car. This allows the current to flow directly into the battery without the car having to convert it.
- Speed: DC charging is much faster. It's suitable when you're on the go and need to charge the car quickly, for example, at highway rest stops.
The charging speed or power being charged into the vehicle is indicated in kilowatts (kW). It indicates how many kilowatt-hours (kWh) can theoretically be charged per hour. Since the vehicle's average consumption is given in kilowatt-hours, this allows for an estimation of the recharged range. The maximum possible charging power is always indicated on both charging cables and charging stations. For AC charging, it ranges from 2.4 kW-44 kW, and for DC charging, between 2.4 kW-500 kW.
What types of AC charging are there?
- Schuko Socket (up to 2.3 kW): Slow charging using a Mode 2 charging cable or a mobility dock. It's more of an emergency solution.
- Wallbox and High-Voltage Socket (3.7–22 kW): Faster charging at home or at campsites using the high-voltage connection with a Mode 2 or Mode 3 charging cable.
- Public AC Charging Stations (11–22 kW): Often found in cities at parking lots, shops, and corporate buildings. Charging is done via a Mode 3 charging cable.
During AC charging, a suitable charging cable is required to reach the desired charging power. The charging power depends on the number of charging lines in the cable:
Single-Phase Charging:
- Power: Typically up to 7.4 kW.
- Voltage: 230 volts.
- Description: This uses one phase of the power grid. This method is widespread and can be used at normal household sockets or special wall boxes. It's the slowest method of AC charging and is suitable for overnight charging or at places where the vehicle is parked for a longer period.
Three-Phase Charging:
- Power: Typically up to 22 kW.
- Voltage: 400 volts.
- Description: Three phases of the power grid are used during three-phase charging, increasing the charging power and thus the charging speed. This method requires special charging equipment, such as wall boxes or public charging stations that support three-phase power.
During AC charging with the Type 2 plug used in Europe, the following charging methods are distinguished:
Mode 3 Charging:
Mode 3 charging is the most common form of AC charging. It involves charging with a cable that has two Type 2 connectors on a charging infrastructure specifically designed for electric mobility. These are used to charge at wall boxes or charging stations.
Mode 2 Charging:
Mode 2 charging is a method for charging electric vehicles, mainly used for charging at home or at locations without special charging infrastructure. This includes typical household sockets but also camping plugs or high-voltage plugs. An important feature of Mode 2 charging is the integrated protection device (ICCB - In-Cable Control Box) built into the charging cable. This box ensures safety by monitoring the charging process and interrupting the power flow in case of problems (e.g., overheating or short circuit). While up to 2.3 kW can be charged at a regular household socket, high-voltage plugs allow up to 22 kW. Since these are different plug types, there are either separate charging cables for the respective plugs or a charging cable that can be modularly upgraded with multiple plug faces.
The charging cable is responsible for communication between the car and the charging station. It determines the charging power for which the On-Board Charger in the car, the charging cable itself, and the charging station are designed. The highest charging power that all participants can provide is then used for the charging process. Therefore, a car can only be charged as quickly as the On-Board Charger and the charging cable allow. Choosing the right charging cable based on the car can thus save money and time.
- Wallbox or Charging Station (3.7-50 kW): At hotels or also in houses
- Fast Charging (50–150 kW): On highways and expressways
- High-Power Charging (HPC) (150–350 kW): Extremely fast charging for long distances, mostly found on highways
During DC charging, a CCS2 charging cable, which is permanently attached to the charging station, is used within Europe. The specified power is provided by the charging cable. Due to the high charging powers flowing into the battery, heat is generated. This heat development and the amount of energy already stored in the battery are transmitted to the charging station via the charging cable to adjust the charging power to the current conditions. This reduction in actual charging power is done automatically and is made to prevent overheating of the battery and associated damage.
To achieve a long battery life, it is often advised to keep the battery mostly in a range between 20-80% of battery capacity. This can prevent several battery-damaging effects. For one, increased heat development occurs while charging above 80%, as a battery operates most efficiently and safely when used in a medium charge range. Additionally, wear and tear are prevented, as very high and very low charge levels can accelerate the chemical aging process of the battery.
Yes, you can use third-party charging cables for your electric car, but there are important safety and compatibility considerations:
When a third-party cable is safe to use
- Most EVs use standardized connectors (Type 2 in Europe, CCS for fast charging), so third-party cables that meet these standards will work.
- If the cable is certified and complies with relevant electrical standards (e.g., IEC, UL), it should be safe for use.
Risks of Using Cheap or Uncertified Cables
- Overheating: If the cable’s ampacity is lower than your charger’s output, it can overheat, damaging insulation and creating fire hazards.
- Loose Connections: Poorly fitting connectors can cause arcing, which damages components and poses safety risks.
- Safety Compliance: Many aftermarket cables sold on online marketplaces fail safety checks—studies show up to 63% of electrical goods online don’t meet standards, and 23% are unsafe.
- Warranty Issues: Using uncertified cables may void your EV or charger warranty.
Best Practices
- Buy from reputable brands or authorized dealers.
- Check for certifications (CE, IEC, UL, or local equivalents).
- Ensure the cable matches your charger’s power rating and connector type.
- Inspect cables regularly for wear or damage.
By handling and maintaining the charging cable correctly, you can ensure that it functions safely and efficiently and has a long lifespan.
Storage:
- Dry Environment: Store the charging cable in a dry place to avoid corrosion and other damage.
- Cleanliness: Keep the cable clean and free from dirt and deposits.
- Orderliness: Roll the cable neatly without tight kinks or knots to avoid damage.
Usage:
- Cable Protection: Avoid pulling the cable over sharp edges or through tight corners that could damage the cable.
- No Overrunning: Ensure that the cable is not run over, as this can damage the insulation and internal wires.
- Protect Connectors: Protect the connectors from water and dirt and avoid dropping or handling them roughly.
Maintenance:
- Regular Inspection: Check the cable regularly for signs of wear, cracks, or other damage.
- Cleaning: Clean the cable contacts regularly with a dry cloth. Do not use aggressive cleaning agents or water.
Usage Instructions:
- Do Not Overstretch: Do not pull on the cable to disconnect it. Hold the plug firmly and pull it straight out.
- Observe Temperature Ranges: Avoid extreme temperatures that could make the cable material brittle or damage it. The charging cables from Lapp can be safely used in temperature ranges between -30°C and +50°C.
- Caution in the Rain: If possible, avoid using the cable in heavy rain to prevent short circuits.
Safety:
- Replace Defective Cables: If the cable is damaged, replace it immediately to avoid electrical hazards.
In order to charge at 22 kW, not only the charging station, but also your car's onboard charger, as well as your charging cable must support 22 kW.
The charging speed of your car is primarily determined by the onboard charger in your vehicle. Not all electric vehicles (EVs) are equipped with a 22 kW AC onboard charger. Many EVs only support lower AC charging rates, such as 11 kW or even 7.4 kW, depending on the model. If your car's onboard AC charger is limited to a lower power output, the car cannot utilize the full 22 kW provided by the charging station. Also, your charging cable may restrict charging speed if it is rated for lower amperage, such as 16 A, instead of 32 A required for 22 kW.The onboard charger (OBC) determines how fast your car can charge from AC sources (home chargers, many public chargers). A higher kW OBC means more power can be converted from AC → DC inside the car.
Example:
- 7.4 kW OBC: adds ~35–50 km range per hour (depending on efficiency).
- 11 kW OBC: adds ~55–75 km range per hour.
- 22 kW OBC: adds ~100–150 km range per hour, but rarely installed in cars.
It has no influence on DC charging since no conversion by the Onboard Charger is required.
The slow charging of your car using a wallbox can be due to several factors. Here are some possible reasons:
- The onboard charger in your car determines the maximum charging power it can accept. If your car only supports 3.7 kW or 7.4 kW charging, even a high-power wallbox (like a 22 kW unit) won't speed up the charging.
- The charging cable you're using must be rated for the power output of the wallbox. If you're using a lower-rated cable, it could limit the charging speed.
- Wallboxes come with different power ratings, typically ranging from 3.7 kW to 22 kW. If your wallbox has a lower power rating, it will charge your car more slowly.
Fast charging allows EV owners to quickly replenish their battery, typically in 30 minutes to an hour, making it highly suitable for long trips and reducing downtime. With more fast-charging stations available, e-mobility becomes more practical and convenient for users. However, fast charging can have several negative impacts on the battery:
- Increased Heat Development: Fast charging generates more heat than slow charging. Excessive heat can affect the chemical processes in the battery and lead to faster aging of the battery.
- Accelerated Wear: Frequent fast charging can accelerate the natural aging process of the battery. The electrochemical reactions occurring at high charging speeds can wear out the anode and cathode more quickly. In addition, charging in extreme heat or cold can increase battery wear, so it is best to only fast charge in moderate weather conditions.
- Reduced Capacity: Over time, frequent fast charging can lead to a faster decrease in battery capacity. This means the vehicle's maximum range is reduced.
- Imbalance in the battery cells: Batteries consist of many individual cells that all need to be charged evenly. Fast charging can make it more difficult to charge the cells evenly, which can lead to imbalances.
Most electric vehicle manufacturers design their batteries to withstand occasional fast charging. Battery management systems (BMS) monitor and protect the battery during fast charging by reducing the charging speed if the battery gets too hot or other problems arise. Nevertheless, it is recommended to balance fast charging with slower methods to maximize battery health and longevity.
Cold (-10°C):
- Reduced battery efficiency leads to higher consumption.
- Range can drop by up to 20–40%.
- Heating the interior consumes additional battery.
- Charging speed decreases.
Heat (+30°C):
- Battery temperature management and air conditioning can cause additional energy consumption.
- Charging power can be throttled to avoid overheating.
Solutions:
- Use pre-conditioning while the car is plugged in.
- Don't drive the battery completely empty, especially in winter.
- Slow charging in winter can be more efficient.
Germany has created a solid foundation for its charging infrastructure, but with the rapid growth of electric mobility, there is still a great need for expansion and optimization. There is still room for improvement, especially in rural areas and with fast charging stations. Nevertheless, investments and political measures show that the charging infrastructure is increasingly being prioritized.
Current status:
- Public charging points:According to data from the Federal Network Agency, as of February 2026 there were over 196,000 public charging points in Germany, of which 146,449 were normal charging points (up to 22 kW) and 49,904 were fast charging points (over 22 kW).
- Fast charging stations:The number of fast charging stations is growing, but varies from region to region. This is particularly important for long-distance journeys.
- Private charging infrastructure:Many households are increasingly installing private wall boxes to enable charging at home, especially in single-family homes.
To achieve the longest possible battery lifespan, it is often recommended to keep the battery mostly within a range of 20-80% of its capacity. This can prevent several battery-damaging effects. As the battery approaches full charge, the charging process becomes less efficient, causing excess heat. This heat can degrade the battery's components over time. Additionally, operating at high charge levels stresses the battery's chemical structure, leading to faster degradation of the lithium-ion cells and reducing overall capacity. To preserve battery health, it is best to charge to 80% for daily use and reserve full charges for longer trips when maximum range is needed.
Yes, for example:
- PlugShare
- Chargemap
- EnBW mobility+
- Tesla Supercharger (for Tesla drivers)