Skip to main content Skip to search Skip to main navigation

Lapp Mobility bronze sponsor at Green Auto Summit 2024 in Stuttgart

Lapp Mobility will be represented as a bronze sponsor at Green Auto Summit in Stuttgart from 21-22 October 2024.

The Green Auto Summit is an important event dealing with the current and future developments of electric mobility. The challenges and opportunities for the industry will be highlighted in numerous lectures and panel discussions. Dr Simon Alig (Managing Director of Lapp Mobility GmbH) will be representing the perspective of charging solution providers.

One of the event's main topics is consumer acceptance and overcoming hurdles such as range anxiety. Discussions on the demand for fast, reliable charging options and the use of data analysis to better understand consumer behaviour are also key topics.

The charging infrastructure for electric vehicles is another key topic at the Green Auto Summit. It forms the backbone of electric mobility and faces major challenges. One important issue is the dependence of infrastructure development on political requirements and regulations. The development of a comprehensive, ultra-fast charging network is also complicated by scalability and implementation problems, especially in connection with integration into smart grids.

Regulatory issues such as the zero-emission requirement by 2035, the EU's Fit for 55 climate package and the significance of subsidies for manufacturers and electric car owners will round off the programme. The Green Auto Summit will thus provide a comprehensive overview of the developments that will shape the future of electric mobility.

Venue: Legends Hall, Graf-Zeppelin-Platz, 71034 Böblingen, Germany

For more information, visit the Green Auto Summit website: https://greenautosummit.com

Skip product gallery

Related products

Mobile charging station Universal SET (up to 11 kW) Type 2 CEE 16A 3-phase + EURO 2-pin plug

Article no.: 5555924001 - Mode 2 Flexible charging: With the Mobile Charging Station Universal SET (up to 11 kW) Type 2 CEE 16A 3-phase + EURO 2-pin plug you can charge your hybrid or electric vehicle flexibly on the road or at home. The Mode 2 charging cable can be connected directly to the mains via the supplied industrial plug or with the household plug included in the SET.  Thanks to an integrated disconnect point, you can also replace the power plug with another power adapter. Thus, with the additionally available 32A 3-phase CEE plug, you can even charge up to 22 kW! In addition, you can also connect your electric car to the power grid in other European countries with the appropriate adapters. However, the mobile charging station Universal SET (up to 11 kW) Type 2 is not only suitable for on the road or in emergencies. It is also a practical addition at home in combination with a wall bracket and can replace a wallbox. With a charging power of up to 11 kW, it can keep up with most wall charging stations. The mobile electric car charging station has an integrated control and protection device in the control box (IC-CPD), which takes charge control via the charging cable to the vehicle. The charging process will stop automatically when the battery is fully charged.   Advantages of the mobile charging station Universal SET (up to 11 kW) Type 2 Technology exchangeable mains adapter Pressure equalization element Ease of use charging at home and on the road at household and industrial sockets no need to set current or parameters automatic termination of charging when battery is fully charged suspension eye on the housing Quality ergonomic, solid plug and socket design robust housing safe to drive over safety VDE certified according to DIN EN 62752:2017 Control box protection class IP67 IEC certified

Regular price: €0.00