Skip to main content Skip to search Skip to main navigation

GOLD FOR THE MOBILITY DOCK: Fourth award within a year

Great success for the MOBILITY DOCK, the innovative charger for electric vehicles from Lapp Mobility. Yesterday it received the coveted German Innovation Award in Gold, and two weeks earlier it had already won the Sustainability Award in Automation.

This means that the MOBILITY DOCK has already won four important awards, as it already received the GERMAN DESIGN AWARD and the eMove360°AWARD in fall 2021. "We are very proud that we have obviously hit a nerve with the MOBILITY DOCK. There was a gap in the range of charging solutions that we were able to close with our innovation," says Frank Hubbert, Managing Director of Lapp Mobility.

A solution that makes our lives better

The German Innovation Award in the highest competition category "Gold" was presented yesterday at a ceremony held by the German Design Council at the Futurium in Berlin. The award recognizes innovative achievements that break new ground through their added value. The focus is on the user experience, with solutions that make our lives better and contribute to a better future.  640 entrants applied for the award. A total of 27 products/projects were awarded the highest distinction of "Gold" - including the MOBILITY DOCK from LAPP.

Sustainability Award in the mobility concepts category

The Sustainability Award in Automation is equally coveted in the industry. It recognizes outstanding examples of sustainable solutions in the areas of environmental and climate protection as well as society and governance in the automotive and mobility industry. It is awarded by the ATZ/MTZ Group and the mobility experts from management consultants Arthur D. Little (ADL) as part of the ATZlive congress "Drives and Energy Systems of Tomorrow 2022" in the three categories of technology, mobility concepts and start-ups. With its MOBILITY DOCK, Lapp Mobility GmbH was one of the winners in the mobility concepts category in the infrastructure sector.

Space-saving, mobile charging station

The jury's enthusiasm for the Mobility Dock is no coincidence. "Our MOBILITY DOCK fully fulfills the function of a mobile charging station, but takes up significantly less space in the trunk," says Frank Hubbert, describing the new product, which was launched in April 2022. The MOBILITY DOCK is a space-saving charger that, in combination with any type 2 charging cable (charging mode 3), allows an electric car to be charged at a standard household socket. This means that electric car drivers need fewer different types of charging cable.

 

Communication from the MOBILITY DOCK to the vehicle takes place via a control unit integrated in the charger, which sets the charging current up to a maximum of 10A and also monitors the charging process. This achieves a maximum charging power of 2.3 kW, which is set automatically. The device monitors the device temperature and the temperature at the household socket. If an increased temperature is detected at the mains plug, the charger automatically regulates the charging power to prevent overheating. As a further protective function for the user, the charger also includes earth conductor monitoring and the detection of DC and AC faults. Such DC and AC faults are detected and protected up to 6mA DC and 30mA AC. The MOBILITY DOCK is CE-compliant and has been developed and tested in accordance with the IEC62752 equipment standard.

 

The Mobility Dock can be ordered from the Lapp Mobility online store.

Skip product gallery

Related products

MOBILITY DOCK - Power plug type E/F (Europe)
MOBILITY DOCK - Power plug type E/F (Europe)

Article no. 5555925000 The MOBILITY DOCK with the power plug type E/F is a small, handy charger, which allows electric and plug-in hybrid vehicles to be charged at any standard household socket in combination with any type 2 charging cable. With the Type 2 socket integrated into the housing, the MOBILITY DOCK is compatible with the European charging cable standard and can be used in the following countries: Austria, Belgium, Bulgaria, Croatia, Czech Republic, Estonia, Finland, France, Germany, Greece, Hungary, Iceland, Italy, Netherlands, Latvia, Lithuania, Luxembourg, Northern Macedonia, Poland, Portugal, Romania, Serbia, Slovakia, Slovenia, Spain and Sweden. The MOBILITY DOCK completely fulfills the function of a mobile charging station, but requires significantly less space in the trunk and can be stowed in the charging floor or in the side pockets of the vehicle to save space. Communication from the MOBILITY DOCK to the vehicle takes place via a control device integrated in the charger, which sets the charging current up to a maximum of 10A and also monitors the charging process. Thus, a charging power up to a maximum of 2.3 kW is achieved, the setting is automatic. The device monitors the device temperature as well as the temperature at the household socket. If an increased temperature is detected at the power plug, the charger automatically regulates the charging power to prevent overheating. As a further protective function for the user, ground wire monitoring and the detection of DC and AC faults are included in the charger. Such DC and AC faults are detected and protected up to 6mA DC and 30mA AC. The MOBILITY DOCK is CE compliant and has been developed and tested in compliance with the IEC62752 equipment standard. To start the charging process, the type 2 charging cable is plugged into the type 2 socket of the MOBILITY DOCK. Then the MOBILITY DOCK with the charging cable plugged in is plugged into the household socket and off it goes. An LED indicates the device status. All components are absolutely stable and firmly anchored. For example, a support is integrated on the side of the device for support against the building wall, which is unlocked by pressing a pushbutton. This allows fine adjustment of the support to the building wall. The plugged-in Mode 3 charging cable is locked to the housing by a mechanism and can be unlocked by the unlocking lever located on the rear side. This allows the Mode 3 charging cable to be pulled out of the charger with little effort. The housing of the MOBILITY DOCK is jet water protected (IP44) and designed for drops from any position from a height of 1m. With its weight of approx. 750g and a size of 255x135x105 mm the MOBILITY DOCK is space and weight optimized. Due to the type 2 socket integrated in the housing, the MOBILITY DOCK is compatible with the European charging cable standard and can be used in the following countries: Austria, Belgium, Bulgaria, Croatia, Czech Republic, Estonia, Finland, France, Germany, Greece, Hungary, Iceland, Italy, Latvia, Lithuania, Luxembourg, Northern Macedonia, Poland, Portugal, Romania, Serbia, Slovakia, Slovenia, Spain and Sweden. The MOBILITY DOCK has already won four major awards. In May 2022, it received the coveted German Innovation Award in Gold and the Sustainability Award in Automation. In fall 2021, the innovative charger received the German Design Award in the Excellent Product Design category and the eMove360°Award 2021 for Electromobility & Autonomous Driving.

Regular price: €259.00
MOBILITY DOCK Set
MOBILITY DOCK Set

Article no. SET-5555925000 With the MOBILITY DOCK set you are perfectly equipped:  With the standard charging cable type 2 (7.4 kW) 5m, black and the MOBILITY DOCK you can charge on the road at any household socket and are not dependent on a charging station. Well stowed in the matching bag, these companions are always neatly packed away in the trunk! The MOBILITY DOCK is a small, handy charger for use on the road that, in combination with any type 2 charging cable, allows electric and plug-in hybrid vehicles to be charged from a standard household socket. The MOBILITY DOCK completely fulfills the function of a mobile charging station, but requires significantly less space in the trunk and can be stowed in the charging floor or in the side pockets of the vehicle to save space. Communication from the MOBILITY DOCK to the vehicle takes place via a control device integrated in the charger, which sets the charging current up to a maximum of 10A and also monitors the charging process. Thus, a charging power up to a maximum of 2.3 kW is achieved, the setting is automatic. The device monitors the device temperature as well as the temperature at the household socket. If an increased temperature is detected at the power plug, the charger automatically regulates the charging power to prevent overheating. As a further protective function for the user, ground wire monitoring and the detection of DC and AC faults are included in the charger. Such DC and AC faults are detected and protected up to 6mA DC and 30mA AC. The MOBILITY DOCK is CE compliant and has been developed and tested in compliance with the IEC62752 equipment standard. To start the charging process, the type 2 charging cable is plugged into the type 2 socket of the MOBILITY DOCK. Then the MOBILITY DOCK with the charging cable plugged in is plugged into the household socket and off it goes. An LED indicates the device status. All components are absolutely stable and firmly anchored. For example, a support is integrated on the side of the device for support against the building wall, which is unlocked by pressing a pushbutton. This allows fine adjustment of the support to the building wall. The plugged-in Mode 3 charging cable is locked to the housing by a mechanism and can be unlocked by the unlocking lever located on the rear side. This allows the Mode 3 charging cable to be pulled out of the charger with little effort. The housing of the MOBILITY DOCK is jet water protected (IP44) and designed for drops from any position from a height of 1m. With its weight of approx. 750g and a size of 255x135x105 mm the MOBILITY DOCK is space and weight optimized. Due to the type 2 socket integrated in the housing, the MOBILITY DOCK is compatible with the European charging cable standard and can be used in the following countries: Austria, Belgium, Bulgaria, Croatia, Czech Republic, Estonia, Finland, France, Germany, Greece, Hungary, Iceland, Italy, Latvia, Lithuania, Luxembourg, Northern Macedonia, Poland, Portugal, Romania, Serbia, Slovakia, Slovenia, Spain and Sweden. The MOBILITY DOCK has already won four major awards. In May 2022, it received the coveted German Innovation Award in Gold and the Sustainability Award in Automation. In fall 2021, the innovative charger received the German Design Award in the Excellent Product Design category and the eMove360°Award 2021 for Electromobility & Autonomous Driving.  

Regular price: €473.00
Mesh bag for the MOBILITY DOCK
Mesh bag for the MOBILITY DOCK

Article no. 5555940001 Storage bag for the MOBILITY DOCK, closable with drawstring and cord stopper, with loop holder for attachment

Regular price: €14.99